請選擇您的送貨地點

國家/地區頁面的選擇會影響各種因素,例如價格、配送方式和產品可用性。
聯絡窗口
台灣易格斯有限公司

igus® Taiwan Company Ltd.

40850 台中市南屯區工業區24路35號5樓

+886 4 2358 1000
+886 4 2358 1100
TW(ZH)

Light and vibration-dampening: bearings in handle dispensers for containers

The iglidur plain bearing allows lightweight and compact machine design in the beverage industry

The "Innopack CSM" uses an application head to provide a wide variety of containers with a handle. Numerous bearing arrangements are used here, which should allow for a lightweight and compact design. Other requirements include low friction values, increased service life, freedom from lubricants, freedom from maintenance, vibration dampening, but also low costs. Here, only plastic plain bearings made of iglidur G and J came into question.

Profile

  • What was needed: Plain bearings made of the materials iglidur G and J
  • Requirements: Low weight, space-saving, reduced manufacturing costs, low friction values, increased service life, freedom from lubrication, maintenance-free and vibration dampening
  • Industry: Packaging industry, beverage packaging
  • Success for the customer: In the pressure sensor system and as roller bearing, the iglidur plain bearings absorb high forces and shocks without any problems. Among other things, they offer a low weight with larger inner diameters than ball bearings, are self-lubricating and insensitive to dirt and dust.
Handle dispenser Application head of the "Innopack CSM" handle dispenser

Problem

The "Innopack CSM" (Carry Strip Master) from KHS Maschinen- und Anlagenbau AG provides containers of all kinds with a handle - from shrink-wrapped cans and PET bottles with and without contours to tetra packs and tray packs. The highly dynamically driven application head, which must be as light and small as possible, is an essential component. The application head of the completely new "Innopack CSM" developed by KHS starts spontaneously as required via a simple pressure sensor system and provides up to 70 containers per minute with a handle. Processing can be carried out in one, two or three lanes - up to 210 containers per minute are possible.
In order to guarantee the high dynamics and positioning accuracy required in operation, the application head was subject to further requirements in addition to the design criteria of "lightweight" and "space-saving": Reduced manufacturing costs, low friction values, increased service life, freedom from lubricants, freedom from maintenance and vibration dampening. The design engineers at KHS were convinced that there was no way around plain bearings and rod ends made of plastic.

Solution

The application head today features several plain bearing applications that absorb high forces and shocks. The bearings are found first in the pivot point for the pressure sensor system and second serve as roller bearings.
Specifically, these are bearings from the iglidur G family, which weigh only little and have larger inner diameters than ball bearings. The economical all-rounders withstand extremely high loads and operate at low to medium surface speeds. The self-lubricating effect makes them maintenance-free in dry operation and insensitive to dust and dirt. As with all iglidur plain bearings, the high-performance material used is composed of base polymer, fibres and fillers as well as solid lubricants. These components ensure that the coefficient of friction and the specific coefficient of wear are set as low as possible. The iglidur G plain bearings also have a good resistance to chemicals. Most lubricants cannot harm them. The same applies to many weak organic and inorganic acids. In addition, iglidur J plain bearings have a particularly low moisture absorption and low coefficients of friction.  The specialist for fast and slow movements ensures very low friction values and the lowest stick-slip tendency in the "Innopack CSM". It is recommended for applications with medium compressive forces - at high speeds and high wear resistance.

"For the conditions stipulated in the specifications regarding weight, space and costs, there was no alternative to the plastic machine elements. The decision for igus as a supplier was also easy for us."
 
Tilo Lechner, responsible for the development of the "Innopack CSM" at KHS Kisters
Handle dispenser

More on applied products here

Further interesting applications from extremely diverse areas can be found here.


名稱 "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" 和 "yes" 是 igus® GmbH/科隆在德意志聯邦共和國以及某些外國適用的情況下受法律保護的商標。這是商標的非詳盡清單(例如igus® GmbH 或igus®在德國、歐盟、美國和/或其他國家或司法管轄區的附屬公司的待審商標申請或註冊商標。

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosh Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mentioned on this website. The products offered by igus® are those of igus® GmbH.