請選擇您的送貨地點

國家/地區頁面的選擇會影響各種因素,例如價格、配送方式和產品可用性。

聯絡窗口
台灣易格斯有限公司

igus® Taiwan Company Ltd.

40850 台中市南屯區工業區24路35號5樓

+886 4 2358 1000
+886 4 2358 1100
TW(ZH)

媒體

您有問題嗎?需要材料嗎?
這裡有最新新聞資訊和可發表的照片材料供您下載。
我們還很歡迎您打電話、發郵件或傳真!
 
媒體聯繫您想要加入我們的媒體發佈列表嗎?

分領域新聞稿

Cables for drive technology found, ordered and connectorised quickly at igus2019/1/3

If the user is looking for a drive cable, then igus, with its portfolio of more than 1,350 cables, always has the optimum solution for the respective application at the most cost-effective price. The motion cable specialist has been developing cables specifically for use in the energy chain for over 30 years and testing them in the largest laboratory for moving applications in the industry. With over two billion test cycles and more than 1.4 million electrical tests per year, igus is the number one for moving cables in energy chains. The new website www.igus.eu/drivenow provides a new gateway to the diverse world of igus cables. From cables sold by the metre and the harnessed, ready-to-connect drive cable with connector up to the special cable in the desired length. The customer has a wide choice. The "Drive" website offers the user a comprehensive overview of the drive technology, the igus test laboratory and the in-house harnessing of cables. In addition, the user has the option to order free samples or directly order the appropriate cable that he wants from the shop.

Tested ready-to-connect cables for motion

All chainflex cable designs have been qualified in a series of extensive tests before the market launch. For example, the TPE servo cable CF29.25.15.02.01.D in Test 5034 withstood 45 million strokes with a bend radius of 7.2 x d. All cables are subjected to a rigorous quality testing programme that even includes batch testing. The jacket materials specifically developed for use in the energy chain offer a wide selection: from PVC and highly oil-resistant PUR up to TPE, the best and most durable material for continuous movement in the energy chain. In addition, the many approvals of cables such as UL, EAC or DNV-GL have the great advantage that the users do not have to obtain their own certificates for the components used and is always safe when exporting machines.

readycable finder helps with quick selection

Upon request igus offers all cables from one source, as a so-called "readycable", tested and with connector. The online tool "readycable finder"helps to select the right drive cable from over 4,200 types according to 24 manufacturer standards, which can then be ordered directly from stock via the online shop. Since all cables are tested in our own test laboratory spread over 2,750 square metres of floor space, igus is the only manufacturer on the market to offer a unique 36-month guarantee on its complete line of cables. The data from the test laboratory is also included in the service life calculator; this gives reliable statements about the durability in the respective application.

名稱 "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" 和 "yes" 是 igus® GmbH/科隆在德意志聯邦共和國以及某些外國適用的情況下受法律保護的商標。這是商標的非詳盡清單(例如igus® GmbH 或igus®在德國、歐盟、美國和/或其他國家或司法管轄區的附屬公司的待審商標申請或註冊商標。

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosh Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mentioned on this website. The products offered by igus® are those of igus® GmbH.