變更語言 :

iglidur are materials developed by igus. They consist of high-performance polymers and are characterised by special specifications. For example, they are exceptionally wear-resistant or suitable for contact with media and chemicals.
But what are iglidur materials made of? And what is behind the self-lubricating effect? Find out more about the specifications and composition of iglidur plain bearings.

選擇合適的平面軸承時,有多種軸承類型可供選擇。每個都有不同的類型和自己的操作模式。我們為您總結了最重要的軸承類型,並向您展示它們具有哪些優勢。

心軸和平面軸承的正確選擇對於軸承系統的良好運作起著決定性作用。平面軸承可保護通常昂貴得多的傳動軸以及軸承點周圍的組件免受磨損。因此,這種磨損僅發生在平面軸承中並及時更換就顯得尤為重要。然而,在設計軸承位置時,常常忽略心軸。了解如何正確地將兩個組件相互匹配。

安裝平面軸承時,需要牢記一些對於無故障運作和長期產品使用壽命至關重要的事項。了解您需要了解的有關合適的安裝和測試方法、間隙設計、標準公差以及平面軸承的正確固定的所有資訊。

What is meant by hydrodynamic and hydrostatic plain bearings? How do these two bearing types work, what are their advantages and what are their typical application areas? Answers to these questions can be found here.

What is tested and how is it tested?
In the iglidur test area, bearings and materials are tested for stress, wear and friction properties. Other parameters such as high and low temperatures, high load and speed are adjusted depending on the test. There are around 50 test systems in the test laboratory, on which more than 300 parallel tests are carried out. At the same time, we carry out around 11,300 tribological tests on the 250 or so newly developed plastic compounds every year. To ensure that the new formulations prove themselves in later use, they are not only exposed to external influences, but also to different directions of movement and loads - rotating, pivoting, linear, tumbling.

親自拜訪:
週一至週五 8:30 - 17:30
線上:
週一至週五 8:30 - 17:30
(可搜尋LINE官方ID-->@igustw)
Online:
24h
若無人在線,可留下您的問題跟聯絡資訊,我們會盡快與您聯繫。
您也可以直接發信到我們共用信箱tw-info@igus.net